2025-02-06 09:52 PM
hi,
I am trying to external loader connect with stm32h723zgt6 + w25q128 .
before loading the stldr file into debugger i need know why cube ide not compiling the data into qspi location ?
In the main.c file constant data has been declared as below .
const __attribute__((section(".extFlash"))) uint8_t buff[] = "Hello world from H723 QSPI";
In the flash id file has been modified as below.
QSPI_FLASH (r) : ORIGIN = 0x90000000, LENGTH = 16M
.extFlash :
{
*(.extFlash)
} >QSPI
after compiling why memory details not showing in the below menu
2025-02-07 12:10 AM
hello,
Try:
uint8_t buff[] __attribute__((section(".extFlash")));
2025-02-07 12:27 AM
hi,
i have modified as below :
uint8_t buff[] __attribute__((section(".extFlash")))= "hello world";
but still problem continues as same !. it not showing as earlier attached picture
2025-02-07 01:07 AM
Have you refreshed the build analyzer? Sometimes it doesn't refresh on its own. Rebuild and click the refresh icon:
Also, why did you remove const? You cannot put a variable in ROM, only constants. The linker won't like it. And if it somehow builds you will get a hardfault error if the MCU tries to modify the object.
Is the object used? If not, it might be optimized away by the linker.
2025-02-07 01:24 AM
hi,
i have modified constant as below
const uint8_t buff[] __attribute__((section(".extFlash"))) = "Hello world from H723 QSPI";
i have refreshed many times and build the project many times but problem is same as continues.
2025-02-07 01:30 AM
Did you use it in your application or you've only declared it? it could be optimized by the tool if you didn't use it.
If you put buff in the live expression are you able to see the content?
2025-02-07 01:37 AM - edited 2025-02-07 01:39 AM
Let me ask again. Is the object used? If not, it might be optimized away by the linker.
Please upload the .map file too.
Please upload the complete linker file too.