2024-09-14 7:00 AM
Two small & easy to do improvement proposals for code generation in CubeMX & IDE:
1. In the message about missing Cube firmware please include after "necessary firmware package" the exact package name with version, to avoid misunderstanding.
2. If option "add necessary library files as reference" is selected - is it possible just to generate the project as if the package were present?
Because no files will be copied. Just create the links/references where the library is assumed to be? User can get the library later.
2024-09-20 9:46 AM
Hello @Pavel A.
Thank you so much for your request. I've escalated it to the concerned team to analyze the possibility of implementation for your request (under internal ticket number 191711).
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.