cancel
Showing results for 
Search instead for 
Did you mean: 

Project (or similar) remains in project tree despite closing the project?

Ricko
Senior

Hi,

I opened one of the examples projects and then closed it. But no matter what I tried (including closing all files and restarting CubeIDE) the FatFS_uSD_Standalone project (or something else?) remains present in the project explorer as if it is some other project. See screenshots below. And there are no options if I right click on it.

 

The icon is also different and cannot find anywhere a summary of CubeIDE icons.

What is that file/project or what does that icon mean? And how do I remove it?

Thank you

Ricko_0-1724892021158.png

 

Ricko_1-1724892216363.png

 

 

 

0 REPLIES 0