2023-05-23 2:51 AM - edited 2023-11-20 4:49 AM
Hello
I've been using the STM32IDE (Windows version) along with NUCLEO 144 boards for 8 months. Now I bought a NUCLEO-L010RB and created a standard project without user code. The build was successful. The program call via RUN and DEBUG generates the following error message.
What is the problem?
what should i do
2023-05-24 2:21 AM
Hello @RMoeh.1
First let me thank you for posting.
Could you provide the debug log for further analysis.
KR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2023-05-24 3:13 AM
2023-05-31 6:56 AM