2020-05-20 04:31 AM
Hello Everybody
I have the Problem with my Hightimer PWM Output.
If I define that my HRTIM is working with 480MHz (CPU_Ck).
it will not and work with the normal 240MHz Output.
Why is that so?
2020-05-20 05:46 AM
Are you trying to get a PWM signal at 240MHz? That's above the max frequency of the GPIO pins.
2020-05-20 07:07 AM
2020-05-20 07:07 AM
2020-05-20 07:07 AM
2020-05-20 08:01 AM
2020-05-20 08:06 AM
Thanks for the answer
No sorry i have made a mistake while i was uploading the pictures
I try to get a faster 10 Bit PWM signal, because of that i need the high resolution timer with 480MHz instead of 240MHz.