cancel
Showing results for 
Search instead for 
Did you mean: 

Problem with FreeRtos in TrustZone enabled

Kendall7
Associate II

Hi 

Hi 

We are using product STM32H56 series , I am encountering problem while building my project 

I am using STM32cubeIDE , trust zone enabled .

I enabled X-CUBE-FREERTOS  M33non secure

In software package I installed   -STm X-CUBE-FREERTOS  -CMSIS RTOS2-TZ_non_secure and desired Heap configuartion .

I am getting the error as below .

Please help me to resolve this issue.

Kendall7_0-1711444735447.pngKendall7_1-1711444777776.png

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
Mahmoud Ben Romdhane
ST Employee

Hello @Kendall7 ,

First let me thank you for posting and welcome to the ST Community.

I suggest that you take a look at this Post .

Thanks.

Mahmoud.

View solution in original post

3 REPLIES 3
Mahmoud Ben Romdhane
ST Employee

Hello @Kendall7 ,

First let me thank you for posting and welcome to the ST Community.

I suggest that you take a look at this Post .

Thanks.

Mahmoud.

Kendall7
Associate II

Hi @Mahmoud Ben Romdhane 

Thank you for responding back to my post!

I already tried the approach listed in this thread Post ,but I was still facing the issue as listed in the post.

Also I am not able to select the "Copy all used libraries into the project folder"

Kendall7_0-1711447628147.png

 

Can you propose a link/Post where the mention problem is solved .

regards,

Kendall.

Hi @Mahmoud Ben Romdhane 

Thank you for responding back to my post!

I am not able to select the "Copy all used libraries into the project folder" so without selecting I did all the steps suggested in the given Post .I am able to Build the project , But is that the right approach .

Can you please guide me on this.

 

Kendall7_1-1711448649031.png

Kendall7_2-1711448782328.png

Thank you.

regards,

kendall