cancel
Showing results for 
Search instead for 
Did you mean: 

Problem when CubeIDE is installed not in default folder and workspace is also not in default path

IKuba
Associate

Hello!

When I install CubeIDE not in default folder and change a folder for workspace there are problems with code generation. This problem occurs with MCUs and Boards. Even if one can generate some code it is not the same code as if the programm and worspace are in default paths. And the debugger does not start...

0 REPLIES 0