cancel
Showing results for 
Search instead for 
Did you mean: 

Problem opening a project CubeIDE

NicRoberts
Associate III

Win 10, x64, STM32CubeIDE version 1.17.0

I'm trying to open a CubeIDE project from a workspace but it just doesn't load, see image below. 

I select the folder for my workspace, click finish & am then told that there are no projects in the folder. Yet the folder does contain a CubeIDE project. The open project option is also greyed out in the projects menu pull down.

What am I missing here?

Cube_Proj_Issue.png

1 ACCEPTED SOLUTION

Accepted Solutions
NicRoberts
Associate III

Turns out I was not in the workspace directory from where the project was created, which was further up the directory hierachy.

View solution in original post

5 REPLIES 5
Peter BENSCH
ST Employee

Please see this thread which probably answers your question.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
NicRoberts
Associate III

Turns out I was not in the workspace directory from where the project was created, which was further up the directory hierachy.

Hello @NicRoberts ,

If you solved your issue please accept your comment as solution.

Thank you.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
JerryMC22
Associate III

I have identical problem with the version 1.17, I also have a lot of problems with version 1.17, I also ghastly sad because of problems of CubeIDE :( really sad.

Hello @JerryMC22 ,

Need to open a separate thread and describe all the problems you are facing.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.