2023-05-15 02:17 AM
Hi, I'm using an STM32F103C8T6 blue pill board with st link programmer
and I want to print a single string hello world
Can we do that with st link or we do need something else to do it ?
thank you for helping
2023-05-16 02:26 AM
Well, that won't really work satisfactorily, because the Blue Pill have been using only fakes for years, which has also been discussed here in the community many times, e.g. here.
If you then also want to use an ST-LINK from one of the cheap suppliers from Asia, the disaster is pre-programmed.
Regards
/Peter
2023-06-19 06:10 AM
Thank you for the answer, I did it with uart communication