2020-03-30 12:01 PM
Hello,
I am new to STM32 dev, so...
Logic analyzer only shows a glitch on MOSI line of SPI1 of around 156 ms then it puts it back to LOW level; similar results for SPI3.
Using PB3 (D23) and PB5 (D22) for SPI3; using PA7 (D11) for SPI1;
Solder bridges: SB49-OFF, SB50-OFF; SB56-ON, SB57-OFF
Checked with DMM for proper connectivity (MCU pin to pin socket)
STM32CubeIDE v 1.3.0
What is commented out has already been tried, and not only that.
Help please!
Thank you
2020-04-02 03:36 AM
I have also tried it like so:
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_DIRECT_SMPS_SUPPLY);
/** Configure the main internal regulator output voltage
*/
// __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Initializes the CPU, AHB and APB busses clocks
*/
__HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW);
__HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSE);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 2;
RCC_OscInitStruct.PLL.PLLN = 64;
RCC_OscInitStruct.PLL.PLLP = 2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 0;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/**Initializes the CPU, AHB and APB busses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
{
Error_Handler();
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_USART3|RCC_PERIPHCLK_FDCAN
|RCC_PERIPHCLK_SPI5|RCC_PERIPHCLK_SPI4
|RCC_PERIPHCLK_SPI1|RCC_PERIPHCLK_SPI2
|RCC_PERIPHCLK_SDMMC|RCC_PERIPHCLK_ADC
|RCC_PERIPHCLK_SPI6;
PeriphClkInitStruct.PLL2.PLL2M = 2;
PeriphClkInitStruct.PLL2.PLL2N = 12;
PeriphClkInitStruct.PLL2.PLL2P = 6;
PeriphClkInitStruct.PLL2.PLL2Q = 2;
PeriphClkInitStruct.PLL2.PLL2R = 2;
PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_3;
PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOMEDIUM;
PeriphClkInitStruct.PLL2.PLL2FRACN = 0;
PeriphClkInitStruct.SdmmcClockSelection = RCC_SDMMCCLKSOURCE_PLL;
PeriphClkInitStruct.Spi123ClockSelection = RCC_SPI123CLKSOURCE_PLL;
PeriphClkInitStruct.Spi45ClockSelection = RCC_SPI45CLKSOURCE_D2PCLK1;
PeriphClkInitStruct.FdcanClockSelection = RCC_FDCANCLKSOURCE_PLL;
PeriphClkInitStruct.Usart234578ClockSelection = RCC_USART234578CLKSOURCE_D2PCLK1;
PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLL2;
PeriphClkInitStruct.Spi6ClockSelection = RCC_SPI6CLKSOURCE_PLL2;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Enable USB Voltage detector
*/
// HAL_PWREx_EnableUSBVoltageDetector();
}
2020-04-04 08:26 AM
Looks like a C/C++ error. In debug mode the C compiler will initialize variables (non-standard behaviour) while the C++ compiler will not. Of course, I am trying to write some ordered C++ code here, which STM32CubeIDE is not too good at.
The problem was with `hspi` handles; solved by initializing them:
LCD_Nokia_5110::LCD_Nokia_5110() :
hspi1({0}),
hspi3({0})
Not having been zeroed, hspi.State was something else than 0 (HAL_SPI_STATE_RESET) and so ` HAL_SPI_MspInit(hspi);` would not get called any more.
These HAL_MSP* callbacks are yet another pain in the game, I did not realize those contained useful code...
I must say that in anticipation to the horrors of this Eclipse based ugliness I spent some 3-4 days trying to port this board in `mbed` and failed. Supporting it there would be much appreciated.