2025-02-11 3:37 AM
Hello all,
I'm experimenting with the Nucleo-N657 board using the ST examples on CubeIDE. I'm finding I can launch the debugger as normal and run it for ages without issues. However when I launch the debugger then next time around, I get "Target not responding". I have to power cycle the board AND restart CubeIDE in order for it to work. I've tried different USB cables and lowering the SWD speed to 1000kHz but no success.
Could this be related to the STM32N6 security? As once I get the target not responding message, not even CubeProgrammer can read the RAM content unless I power cycle. I just don't understand having to close and re-open CubeIDE.
Any help would be appreciated. Thanks.