2023-10-01 9:29 AM
Here is my code and I encountered the error. I use H7A3ZI-Q board
/* USER CODE BEGIN Header */
/**
******************************************************************************
* @file : main.c
* @brief : Main program body
******************************************************************************
* @attention
*
* <h2><center>© Copyright (c) 2019 STMicroelectronics.
* All rights reserved.</center></h2>
*
* This software component is licensed by ST under BSD 3-Clause license,
* the "License"; You may not use this file except in compliance with the
* License. You may obtain a copy of the License at:
* opensource.org/licenses/BSD-3-Clause
*
******************************************************************************
*/
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <string.h>
#include <stdio.h>
/* USER CODE END Includes */
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
/* USER CODE END PTD */
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
/* USER CODE END PM */
/* Private variables ---------------------------------------------------------*/
I2C_HandleTypeDef hi2c1;
UART_HandleTypeDef huart2;
/* USER CODE BEGIN PV */
static const uint8_t TMP102_ADDR = 0x48 << 1; // Use 8-bit address
static const uint8_t REG_TEMP = 0x00;
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART2_UART_Init(void);
static void MX_I2C1_Init(void);
/* USER CODE BEGIN PFP */
/* USER CODE END PFP */
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
/**
* @brief The application entry point.
* @retval int
*/
int main(void)
{
/* USER CODE BEGIN 1 */
HAL_StatusTypeDef ret;
uint8_t buf[12];
int16_t val;
float temp_c;
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART2_UART_Init();
MX_I2C1_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
// Tell TMP102 that we want to read from the temperature register
buf[0] = REG_TEMP;
ret = HAL_I2C_Master_Transmit(&hi2c1, TMP102_ADDR, buf, 1, HAL_MAX_DELAY);
if ( ret != HAL_OK ) {
strcpy((char*)buf, "Error Tx\r\n");
} else {
// Read 2 bytes from the temperature register
ret = HAL_I2C_Master_Receive(&hi2c1, TMP102_ADDR, buf, 2, HAL_MAX_DELAY);
if ( ret != HAL_OK ) {
strcpy((char*)buf, "Error Rx\r\n");
} else {
//Combine the bytes
val = ((int16_t)buf[0] << 4) | (buf[1] >> 4);
// Convert to 2's complement, since temperature can be negative
if ( val > 0x7FF ) {
val |= 0xF000;
}
// Convert to float temperature value (Celsius)
temp_c = val * 0.0625;
// Convert temperature to decimal format
temp_c *= 100;
sprintf((char*)buf,
"%u.%u C\r\n",
((unsigned int)temp_c / 100),
((unsigned int)temp_c % 100));
}
}
// Send out buffer (temperature or error message)
HAL_UART_Transmit(&huart2, buf, strlen((char*)buf), HAL_MAX_DELAY);
// Wait
HAL_Delay(500);
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
// Rest of auto-generated Cube functions
// ...
Solved! Go to Solution.
2023-10-01 10:10 AM
Is MX_GPIO_Init defined? The error suggests it isn't. If it is, attach your IOC file. Attaching the full main.c file would be helpful too. Could be a bracket mismatch issue.
2023-10-01 10:10 AM
Is MX_GPIO_Init defined? The error suggests it isn't. If it is, attach your IOC file. Attaching the full main.c file would be helpful too. Could be a bracket mismatch issue.
2023-10-02 7:56 AM
2023-10-02 8:00 AM
Okay, so it's not defined in main.c, but neither are your other MX_*_Init calls. Is it defined in gpio.c?
Your stm1.PNG file doesn't load, and you didn't attach the IOC which would be needed to investigate further.
2023-10-02 8:10 AM
I don't know why I can not upload my ioc file
2023-10-02 8:14 AM
2023-10-02 11:44 AM
ST's forum software often doesn't let people attach IOCs for some reason. Feel free to leave negative feedback in the Feedback Forum.
Can't really offer much other help without that, other than suggesting updating to the latest version of things, if you're not already there.