2022-03-29 8:35 AM
Hi. Can you say me what mean that type of error.
The code is surely correct because I've been working on it. The errors showed up after updating CubeIDE to a new version and generating files from .ioc file in IDE.
c:\st\stm32cubeide_1.7.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.10.3-2021.10.win32_1.0.0.202111181127\tools\arm-none-eabi\bin\ld.exe: ./Core/Src/communication/sms.o:C:/master_g474ve/Debug/../Core/Inc/config.h:54: multiple definition of `config'; ./Core/Src/battery_charger.o:C:/master_g474ve/Debug/../Core/Inc/config.h:54: first defined here
Solved! Go to Solution.
2022-03-29 10:04 AM
Probably this:
2022-03-29 9:23 AM
Is config.h a CubeMX generated file? Certainly neither sms.c nor battery_charger.c is.
Probably you have the "config" variable/function defined in config.h, which is being included in two compilation units, which leads to duplicate definitions.
Move your definitions into source files and keep only the declaration in the header.
> The code is surely correct because I've been working on it.
Not sure that logic tracks.
2022-03-29 10:04 AM
Probably this:
2022-03-29 11:53 PM
Yes. It's answer to my question
2023-07-17 10:35 PM - edited 2023-07-17 10:36 PM
Please go through https://gcc.gnu.org/gcc-10/porting_to.html
In STM32CubeIDE, Goto Project Properties-> --> C/C++ Build -->Settings--> MCU GCC Compiler--> Miscellaneous--> other flags --> Add -fcommon Apply and Close.
Hope this will help.
2024-09-27 2:47 AM
Hallo Mitarbeiter II, das hat bei mir geholfen, es kam die Fehlermeldung, einer doppelten Definition in einer .o Datei.
-fcommon eingetragen, und keine Fehlermeldung mehr, GENIAL. Was bewirkt dieser Eintrag ? Danke nochmal von ganzem Herzen. Liebe Grüße
2024-09-27 2:59 AM
Habe gerade den Link gelesen, alles klar, danke.