cancel
Showing results for 
Search instead for 
Did you mean: 

Missed files when 'Enable BASEPRI support' in X-CUBE-AZRTOS-F7'

diverger
Senior

Hi,

It seems the X-CUBE-AZRTOS-F7 1.1.0 is based on ThreadX 6.1.7. But after select 'Enable BASEPRI support', it missed several files which exist in the official 6.1.7 release, they are:

tx_thread_interrupt_disable.S and _tx_thread_interrupt_restore.S.

Thanks.

 

'

1 REPLY 1
Mahmoud Ben Romdhane
ST Employee

Hello @diverger ,

First let me thank you for posting.

I have created a project with STM32F722ICK6 and I have installed and enabled X-CUBE-AZRTOS-F7.

 

MahmoudBenRomdhane_0-1737554367491.png

 

tx_thread_interrupt_disable.S and _tx_thread_interrupt_restore.S are well generated.

MahmoudBenRomdhane_1-1737554729200.png

 

Thanks.

Mahmoud