2024-09-09 01:45 AM - last edited on 2024-09-09 02:23 AM by SofLit
hi
I use touchgfx 4.24 , STM32CubeIDE 1.16 and STM32cubeMX 6.12
I do a project with touchgfx, I import it on cubeide, no problems to launch it on the card (STM32F769I-DISCO)
I make a modification ( uart 5) on the file ioc and the bilioteque (newlib rentrand) as requested by CubeMX. When I launch after compilation I have an error, of type MemManage_Handler
I do not see mistake that I could have comeate.
Who can help me?
thank
2024-09-09 03:21 AM - edited 2024-09-09 03:22 AM
Hello @pascalous and welcome to the community,
Check the MPU config and if you declared something in a memory region that MPU prevents that access.