Skip to main content
Visitor II
September 25, 2024
Question

STM32U5G9J-DK2)ThreadX example project compilation errors in IAR

  • September 25, 2024
  • 0 replies
  • 838 views
I am getting the following error when compiling the Thread X example project for STM32U5G9J-DK2 in IAR. 
 
Error[Lt069]: The module Font.o(touchgfx_core.a) (and 42 more) has DSP-support enabled, but the current CPU does not.

The procedure i took to get here was:

 

1. Open up TouchGFX and start new project using the example

2. Generate code using TouchGFX

3. Open up the STMCube file and change the IDE from CubeIDE to IAR

4. Generate the code from STMCube

5. Regenerate the code using touchGFX

6. Compile in IAR.

 

I am running TouchGFX 4.24.1 and IAR 9.50.1

This topic has been closed for replies.