cancel
Showing results for 
Search instead for 
Did you mean: 

mbedtls_hardware_poll implementation is incorrect

JCHABOD
Associate

Hi,

I am using MBEDTLS/LWIP/FREERTOS on STMCube Ide v1.10.0

I noticed by calling manually `mbedtls_hardware_poll` that the returned values are only random by group of 4 chars:

When asking for 32 random bytes, the buffer returned is the following:

res=[62 62 62 62 78 78 78 78 49 49 49 49 D9 D9 D9 D9 80 80 80 80 E8 E8 E8 E8 FB FB FB FB 0E 0E 0E 0E ]

Here is the generated code:

 

 

int mbedtls_hardware_poll( void *Data, unsigned char *Output, size_t Len, size_t *oLen ) { uint32_t index; uint32_t randomValue; for (index = 0; index < Len/4; index++) { if (HAL_RNG_GenerateRandomNumber(&hrng, &randomValue) == HAL_OK) { *oLen += 4; memset(&(Output[index * 4]), (int)randomValue, 4); } else { Error_Handler(); } } return 0; }

 

But the memset will write every 32-bit word with only 8 random bits (See `memset` page : the `c` parameter is int but the filled value uses it as a char.

Replacing the `memset` line by the following line seems to fix the issue:

 

memcpy(&(Output[index * 4]), &randomValue, 4);

 

And now the returned buffer is:

res=[50 4E C4 1E DD E5 E0 BC 76 74 3D 93 A6 FD A6 D8 F4 15 8C D4 86 86 45 C6 F9 D6 AB 12 81 37 06 5E ]

Note that I have also checked that the generated code under Ide v1.13.0 is the same

0 REPLIES 0