cancel
Showing results for 
Search instead for 
Did you mean: 

library compiled for stm32F4 series compatible for custom Cortex M4?

dwarakanath
Associate

Edited to clarify that this is specifically STM32F4 (originally just said "Fx").


I've a library .a file compiled using STM32CubeIDE for STM32F4 series.

Is the .a file be compatible to Custom ARM Cortex M4 to use in IAR Embedded Work bench?

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Yes, if it doesn't include anything STM32F4-specific, it should work on other Cortex-M4 processors. Something like a DSP library would be compatible.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

8 REPLIES 8
Andrew Neil
Super User

There's two independent questions there:

  1. Is the .a library compatible with this "Custom ARM Cortex M4" ?
    I guess if the Custom part has the exact same options as in the STM32Fx, it should work.
     
  2. Can IAR use a GCC .a library created by CubeIDE ?
    You would have to ask IAR that one:
    https://www.iar.com/support 

If you have the source, surely rebuilding from source would be the safest option?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
KnarfB
Super User

Fx can be Cortex-M0 or Cortex-M4.

"Custom  ARM Cortex M4" could have other HW features implemented than STM32.

Also check the floating point options which are used on either side.

hth

KnarfB


@KnarfB wrote:

Fx can be Cortex-M0 or Cortex-M4.


Also M3, M33, M7, M55:

AndrewNeil_0-1750243613546.png

 

@dwarakanath so did you mean F4 ?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hi @Andrew Neil 

Yes. F4 here in my case.

Also the .a file doesn't have any peripheral related inclusions. Its purely some algo part.

@KnarfB 

No float support in either the cores.


@dwarakanath wrote:

Yes. F4 here in my case.


OK - I'll edit the title to clarify.

 


@dwarakanath wrote:

Also the .a file doesn't have any peripheral related inclusions. Its purely some algo part.


But there are still optional features & configuration options in the core itself.

You'd have to make sure they all match.

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
Super User

Yes, if it doesn't include anything STM32F4-specific, it should work on other Cortex-M4 processors. Something like a DSP library would be compatible.

If you feel a post has answered your question, please click "Accept as Solution".

Let me check and update 

It didn't work. some stack related linking error popped up. I think this is compiler dependent.

 

Thanks folks for the encouraging support.