cancel
Showing results for 
Search instead for 
Did you mean: 

LED Blink - STM32F429I-DISCOVERY TIM1

Ayoubassame
Associate
could somebody please help me with this: i am a beginner ,i have done the clock configuration and Timer configuration  for delay and also the GPIO configuration: the LED does blink but instead of 1s it takes like 4s , i have done a lot of research to find out where the problem might be, but found nothing i use STM32F429i discovery by the way . thank you and here is my code :

 

void Clock_Config(void) { RCC->CR |=(RCC_CR_HSEON); while(!((RCC->CR) & (RCC_CR_HSERDY))); RCC->APB1ENR |= (1<<28); PWR->CR |= 1<<14; FLASH->ACR |= (1<<8)|(1<<9)|(1<<10)|(2<<0); RCC->CFGR|=RCC_CFGR_HPRE_DIV1; RCC->CFGR |= RCC_CFGR_PPRE1_DIV4; RCC->CFGR |= RCC_CFGR_PPRE2_DIV2; RCC->PLLCFGR |= (0<<16)|(4<<0)|(180<<6)|(RCC_PLLCFGR_PLLSRC_HSE); RCC->CR |=(RCC_CR_PLLON); while(!((RCC->CR) & (RCC_CR_PLLRDY))); RCC->CFGR |=(RCC_CFGR_SW_PLL); while ((RCC->CFGR & RCC_CFGR_SWS) != RCC_CFGR_SWS_PLL); } void Timer_Config(void) { RCC->APB2ENR|=(1<<0); TIM1->PSC=180-1; TIM1->ARR=0xffff; TIM1->CR1|=1<<0; while (!((TIM1->SR)& (1<<0))); } void Delay_µs(int µs) { TIM1->CNT=0; while (TIM1->CNT<µs); } void Delay_ms (int ms) { for (uint16_t counter=0;counter<ms;counter++) { Delay_µs(1000); } } void GPIOxConfig(void) { RCC->AHB1ENR |=(1<<6); GPIOG->MODER|=(1<<26)|(1<<28); GPIOG->OTYPER&=~(0<<13)|~(1<<14); GPIOG->OSPEEDR |=(2<<26) | (2<<28) ; GPIOG->PUPDR&=~((1<<26) | (1<<28)); }
View more

 

1 ACCEPTED SOLUTION

Accepted Solutions

Have the STM32 print out the AHB, and APB clocks.

Inspect the internal frequencies via PA8 MCO pin on a scope.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

3 REPLIES 3

>> i am a beginner

Ok, but this communicates no information about what you do know, or if you're just 14. Register level coding does imply some reading / interpretation of the technical manual.

TIM1 / APB2 is likely not clocking at 180 MHz, but a fraction of that. So perhaps 90 or 45 MHz ? Check the divider settings and Clock Tree, in this context.

Also Toggling will further half the frequency (double the period) of a blinking LED

APB1 DIV4 is 45 MHz, TIMCLK= APB1*2, so 90 MHz

So 1000 delay is 2 seconds, LED ON at 4 second interval ?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

i checked the Clock tree, the APB2 bus is working on 180 Mhz , and in the Timer configuration in PSC register i wrote 180-1, that means 180Mhz divided by 180 is 1Mhz which is 1 tick in on microsecond STM32CubeMX Untitled__ STM32F429ZITx STM32F429I-DISC1 07.06.2024 15_42_38.png

Have the STM32 print out the AHB, and APB clocks.

Inspect the internal frequencies via PA8 MCO pin on a scope.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..