cancel
Showing results for 
Search instead for 
Did you mean: 

Issue when updating from the repository with version 1.7.0

MScac.11
Associate II

I'm having the following error when reloading or updating from the repository:

eclipse.buildId=Version 1.7.0

java.version=11.0.10

java.vendor=AdoptOpenJDK

BootLoader constants: OS=macosx, ARCH=x86_64, WS=cocoa, NL=en_IT

Framework arguments: -keyring /Users/marcelloscacchetti/.eclipse_keyring

Command-line arguments: -os macosx -ws cocoa -arch x86_64 -keyring /Users/marcelloscacchetti/.eclipse_keyring

org.eclipse.equinox.p2.metadata.repository

Error

Sun Jul 25 12:40:27 CEST 2021

No repository found at https://sw-center.st.com/stm32cubeide/updatesite1.

I've cleared all caches, restarted, removed and re-added the repositories.

Any suggestion?

1 ACCEPTED SOLUTION

Accepted Solutions
Julien D
ST Employee

The outage should now be resolved.

You may have to manually Reload the software site from the Preferences:

0693W00000D0a2ZQAR.png 

And if still don't work, clean your cache as described in link shared by @TDK​ .

View solution in original post

6 REPLIES 6
TDK
Guru
MScac.11
Associate II

I did, including completely unistall, delete all eclipse-related folders, seems nothing is making a difference. The post you linked seems to mention a 404 error, I'm getting an access denied error. I don't know if they relate to the same issue...

P.S: no proxy or anything just a straight network connection

Julien D
ST Employee

Fyi, we experiencing issues with all connections to sw-center.st.com. We'll update this thread once resolved.

Julien D
ST Employee

The outage should now be resolved.

You may have to manually Reload the software site from the Preferences:

0693W00000D0a2ZQAR.png 

And if still don't work, clean your cache as described in link shared by @TDK​ .

MScac.11
Associate II

Great I can confirm this is working now. Thanks Julien.

Perfect, can you confirm this topic been fixed using the "select as best" feature on the reply. Thanks by advance.