2021-07-25 3:43 AM
I'm having the following error when reloading or updating from the repository:
eclipse.buildId=Version 1.7.0
java.version=11.0.10
java.vendor=AdoptOpenJDK
BootLoader constants: OS=macosx, ARCH=x86_64, WS=cocoa, NL=en_IT
Framework arguments: -keyring /Users/marcelloscacchetti/.eclipse_keyring
Command-line arguments: -os macosx -ws cocoa -arch x86_64 -keyring /Users/marcelloscacchetti/.eclipse_keyring
org.eclipse.equinox.p2.metadata.repository
Error
Sun Jul 25 12:40:27 CEST 2021
No repository found at https://sw-center.st.com/stm32cubeide/updatesite1.
I've cleared all caches, restarted, removed and re-added the repositories.
Any suggestion?
Solved! Go to Solution.
2021-07-26 12:22 AM
The outage should now be resolved.
You may have to manually Reload the software site from the Preferences:
And if still don't work, clean your cache as described in link shared by @TDK .
2021-07-25 8:03 AM
Could be a cache issue.
2021-07-25 11:10 AM
I did, including completely unistall, delete all eclipse-related folders, seems nothing is making a difference. The post you linked seems to mention a 404 error, I'm getting an access denied error. I don't know if they relate to the same issue...
P.S: no proxy or anything just a straight network connection
2021-07-25 11:17 PM
Fyi, we experiencing issues with all connections to sw-center.st.com. We'll update this thread once resolved.
2021-07-26 12:22 AM
The outage should now be resolved.
You may have to manually Reload the software site from the Preferences:
And if still don't work, clean your cache as described in link shared by @TDK .
2021-07-26 1:05 AM
Great I can confirm this is working now. Thanks Julien.
2021-07-26 1:10 AM
Perfect, can you confirm this topic been fixed using the "select as best" feature on the reply. Thanks by advance.