2025-01-24 1:39 AM
Hi
"I am using the STM32F407 to interface with the ISM330DHCX. I have installed the X-CUBE MEMS1 package, configured the SPI1 protocol, and generated the code. However, I have absolutely no idea how to initialize and use the sensor in my main.c code. How should I write the code correctly?" Let me know some suggestions.
2025-01-29 3:30 AM
Hi @Kumar123,
You can refer to this detailed article on How to integrate the X-CUBE-MEMS1 package with your project and also to this article How to install and import an X-CUBE Expansion Package with STM32CubeMX.
Thank you.
ELABI.1
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-01-29 8:54 PM
Hi ELABI.1
"I've written the logic based on the example, but the values aren't being generated as expected."