cancel
Showing results for 
Search instead for 
Did you mean: 

ioc file not generating

Srinath_03
Senior

hi i have been trying to configure mcu of h745BIT3 208 pin, IOC file is not generating, and i have tried for g4 series same issue happening today only, is there any server down or update have to do.

 

 

regards,

srinath

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @Srinath_03 

Actually, @Andrew Neil ’s reply is very helpful. Please check the provided links and try the suggested workaround; it should help you resolve the issue.

I will be waiting for your feedback.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6
Ghofrane GSOURI
ST Employee

Hello @Srinath_03 

Could you please provide more details about STM32CubeIDE version that you are using also your OS.

THX
Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

windows 11 and stm32cube ide version 1.16.1

 and my friend's laptop windows 11 and version 1.17 both the systems IOC file is not generating

 

 

 

regards,

srinath

Andrew Neil
Super User

Did you see these recent posts:

v1.16.0: STM32Cube Option disabled during project creation; No .ioc File Generated

stm32 targeted project type is empty and its not generating .ioc file

CubeIDE 18.1 does not create CubeMX project - no .ioc file

 

 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

Hello @Srinath_03 

Actually, @Andrew Neil ’s reply is very helpful. Please check the provided links and try the suggested workaround; it should help you resolve the issue.

I will be waiting for your feedback.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi @Ghofrane GSOURI after updating stm32cubeide to 1.19.0 version it works fine.

do you know why suddenly old version is not supporting the ioc file generation? 

regards,

srinath

hi @Andrew Neil thanks for your response it solved the issue after updating the cube ide.

regards,

srinath