2020-05-03 2:51 AM - last edited on 2024-10-10 8:16 AM by Andrew Neil
Is there anyway to increase the size of the icons in the top menu bar in the IDE?
I am 70 now and my eyesight needs a wake-up here :)
2020-05-03 6:09 AM
Not apart from changing the resolution of your screen, or tinkering with the internals, sadly.
2020-05-03 7:42 AM
Just track down the real program (not the launcher) and override it's DPI scaling.
2023-04-08 6:27 PM - edited 2023-11-20 9:29 AM
Beside this question like to be slightly outdated I found a neat solution to this issue.
I've the same problem when running STM32CubeIDE (Eclipse 4.23) under Linux on a 4k screen.
It's described here and seems to work: https://askubuntu.com/questions/777411/eclipse-neon-icon-size-in-ubuntu-16-04-hidpi
So I've edited the /usr/share/applications/stm32cubeide.desktop by adding `GDK_DPI_SCALE=0.5 GDK_SCALE=2` to the line beginning with Exec=....
The full line is now
`Exec=GDK_DPI_SCALE=0.5 GDK_SCALE=2 stm32cubeide %F`
The difference:
STM32CubeIDE on a 4k screen without any specific GDK settings
The same with modified GDK-settings:
Hope it helps if someone is searching for a solution.
BTW, the often mentioned solution `-Dswt.autoScale=175` or similar does NOT work. It only works on older Eclipse versions (prior 4.8?).
2024-10-10 8:13 AM
Not sure if this answer already exists, but just hope to help whoever lands on this question in the future. :)
On Windows 11, you can change the properties of the executable file to make the icons bigger.
1. Find your STM32CubeIDE shortcut -> RIGHT CLICK -> Open file location
2. Open the properties of the .exe file
3. Navigate to "Compatibility" on the pop-up
4. Under "Settings", click "Change high DPI settings" button
5. Under High DPI scaling override, check the "Override high DPI scaling behavior." checkbox
6. Select "System" in the drop-down menu
7. Click OK -> Apply
8. Restart the IDE
Hopefully that solved the problem.
2025-01-28 12:14 PM
My 75 year old eyes Thank You!