cancel
Showing results for 
Search instead for 
Did you mean: 

In the CubeIDE 1.7.0 development environment, I encountered a problem while recording in a flash

when trying to write the firmware to the flash of the controller, an error is displayed that the program cannot connect to the flash. At the same time, the CubeProg controller sees, reads, flashes. In Keil ver. 25, everything is fine, in older versions, a warning about the problem is first displayed, but pressing the flash button again starts the recording process or debug mode.

0 REPLIES 0