2022-01-28 1:57 AM
I want to create my own external loader for STM32U585. So I start with importing IS61WV51216BLL_STM3210E-EVAL (TrueStudio) to STM32CubeIDE. Tis works in principle, but when linking the project I get the error:
update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: Loader/Dev_Inf.o:(.rodata+0x0): multiple definition of `StorageInfo'; ./Loader/Dev_Inf.o:(.rodata+0x0): first defined here
When I comment the line " KEEP(Loader/Dev_Inf.o ( .rodata ))" in stm32_flash.ld file everything compiles fine, but header with storage info is missing in elf file (*.stldr)
2022-01-28 6:17 AM
You need KEEP as there's no internal reference to the structure.
The Linkers complaining you've defined it TWICE, or more, figure out why that's happening, for example you've defined it in a .H file and included that in multiple places. Don't define/allocate things in Include files...
2022-02-08 10:59 PM
The same thing happened to me. The project was working fine with IDE 1.6.0, but after updating it to 1.8.0 it does not work anymore. I am still figuring it out why.
2022-02-28 2:03 AM
Hello, I have had the same problem, working with 1.5.0, but no more working with 1.8.0.
Have you found something to make this work again?
Thanks,
Marco
2022-03-09 11:39 PM
Yes, I use this linker script.
https://github.com/cturvey/stm32extldr/blob/main/ExternalLoader.ld
But unfortunately external loaders only work with ST-LINK, not with USB bootloader.
So now I write my own bootloader.
2024-11-23 4:26 AM
Guys, dont forget to uncheck those before generating code; for removing static declaration from the external call functions. Those for example, refer to attached picture.