User Activity

 In STM32CubeIDE Version: 1.17.0 Build: 23558_20241125_2245 (UTC) (migrate from FW_H7 V1.11.2 to FW_H7 V1.12.0), the ADC3 initialization code generated from the .ioc file is missing the resolution setting. Specifically, the line hadc3.Init.Resolution...
After updating to STM32CubeIDE Version: 1.16.0 Build: 21983_20240628_1741 (UTC), I've noticed that HAL_ADC_Init is being called twice. This behavior is different from the previous version 1.15, where it was called only once. Although the code still f...
Kudos given to