cancel
Showing results for 
Search instead for 
Did you mean: 

If possible, how do you change the pin mapping of auto-generated code in STM32Cube?

BrianG
Associate II

I'm wanting to create a project for the Murata LoRa typABZ module, which appears to use the STM32L082CZU with UFQFPN48 package. In the IDE, I get the message: "The target device 'STM32L082CZUx' is currently not supported by STM32CubeIDE". I started a project using STM32L082CZY, but the pin mapping is different and somethings are not working. I don't see where, but can I change this mapping or is it more complicated than that? Or, is there a another way to auto-generate for this part? Will this be supported in the near future?

1 REPLY 1
dbgarasiya
Senior II

you can change in .ioc file (hardware file)