cancel
Showing results for 
Search instead for 
Did you mean: 

I'm working with ubuntu and it gives me the following error doing debug

DQuir.1
Associate II

Could not determine GDB version using command: /opt/st/stm32cubeide_1.2.0/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.linux64_1.0.0.201904181610/tools/bin/arm-none-eabi-gdb --version

/opt/st/stm32cubeide_1.2.0/plugins/com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.linux64_1.0.0.201904181610/tools/bin/arm-none-eabi-gdb: error while loading shared libraries: libncurses.so.5: cannot open shared object file: No such file or directory

26 REPLIES 26

my Ubuntu Version is 24.04 LTS 

and its not working 

 

Screenshot from 2024-05-04 21-48-10.png

Thank you, still working on Ubuntu 24.04

Many thanks very usefull

Thanks! Adding the repository was the solution for me.

Hope ST fixes next versions in order to use libncurses6

I'm getting the same error but when I try the above command I get "unable to locate package libncurses5"????

 

DAldr.1
Associate II

ST has a real problem here as evidenced by the number of respondents.  What needs to happen ASAP is a rebuild using libncurses.so.6.  Looking across the net, it appears that 6 alleviates some long existing security issues.  Version 5 is not even on option in my Mint/Ubuntu 22 Kernel 6.8 distribution.  I finally resulted begrudgingly, to drop back to windows.

 

Good Luck All.

Object-Option not available in my distribution.