2021-11-26 8:47 AM
Error in final launch sequence:
Failed to start GDB server
Failed to start GDB server
Error in initializing ST-LINK device.
Reason: (4) No device found on target.
2021-11-26 10:43 AM
Hi GAcqu,
This error means CubeIDE was able to find your ST-Link device, but no target chip connected to it. Are you using a Nucleo? If so, are the jumpers on the board connected properly?
Kind regards,
moatjon
2021-11-29 1:01 AM
Hello @GAcqu.1 and welcome to the Community :)
Can you connect with STM32CubeProgrammer?
Make sure to update the ST-link firmware.
Check the USB cable, jumpers. You can try a different cable and/or USB port, boards.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Imen
2021-12-10 1:45 AM
Hi @GAcqu.1 ,
Were you able to resolve the issue ?
Please share your progress or resolution with the community here, so that more members can benefit from this discussion.
Thanks
Imen