I get an error when debugging with Cube IDE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-04 6:44 PM
Thank you for helping.
environment:
STM32CubeIDE Ver1.6.0
When I start debugging with the STM32Cube IDE, I get the following error:
Please tell me what to do.
Thank you.
-----
STMicroelectronics ST-LINK GDB server. Version 5.8.0
Copyright (c) 2020, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
InitWhile : Enabled
Waiting for debugger connection...
Debugger connected
-------------------------------------------------------------------
STM32CubeProgrammer v2.7.0-RC1
-------------------------------------------------------------------
ST-LINK SN : 003D00283137511533333639
ST-LINK FW : V3J7M2
Board : STLINK-V3MINI
Voltage : 3.26V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x451
Revision ID : Rev Z
Device name : STM32F76x/STM32F77x
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a03996.srec
File : ST-LINK_GDB_server_a03996.srec
Size : 8303424 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 5]
Erasing memory corresponding to segment 1:
Erasing external memory sectors [0 120]
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:36.047
Verifying ...
Error: Data mismatch found at address 0x080571B8 (byte = 0x7B instead of 0x63)
Error: Download verification failed
Encountered Error when opening C:\ST\STM32CubeIDE_1.6.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.6.0.202101291314\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
- Labels:
-
STM32CubeIDE
-
STM32F7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-05 3:38 AM
Hello
check if Vcc pins have the proper capacitors connected (0.1 + 4.7 μf), Vcap1 , Vcap2 connected with 2.2μF capacitors. VDDA, VREF are connected properly(usualy to vcc).
Is the error persistent to the 0x080571B8 address?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-05 3:44 AM
Simply your verify in flash report error on memory, but maybe isnt real.
Try slow down speed
SWD freq : 24000 KHz
is high and need perfect powering, cabling and pcb routing. In debuger window setup no AUTO speed
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-05 12:33 PM
Is the device protected?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-04-06 4:57 PM
Thank you for helping.
Thank you for your reply.
The board is custom, but I was able to debug it a while ago.
I recently replaced the host machine. (Windows10-> Windows10)
Can it affect you?
Also, with CubeProgrammer v2.7.0, I was able to confirm that it connects at 24000kHz.
What could be the reason why you can connect with CubeProgrammer but not with CubeIDE?
You can also connect at CubeIDE ST-LINK (OpenOCD) 8000kHz.
What could be the reason why you can connect with ST-LINK (OpenOCD) of CubeIDE but not with ST-LINK (GDB server)?
Can you please explain the difference between OpenOCD and GDB Server?
Thank you.