2021-11-18 11:38 PM
Hi Genius,
I am using STM32G081T6 with STM32cubeIDE. I found out in pinout & configuration setting, there are several USART modes including Single Wire (half-duplex). I set baud rate to 1200, word length to 7Bits, parity even and 1 stop bit. Then connect the single pin with arduino maker nano who already tested with real SDI-12 sensor. I ping dummy msg from arduino to stm32 but doesn't get expected value. Guide me to solve this, there might be something that I missed
Thanks in advanced
2021-11-19 5:13 AM
The number of data bits includes parity, so you will need to set 8 bits if you have 7 data bits.
Single wire is nontrivial, as the two devices need to be in sync in order not to talk over each other. Show the code you're using.
2021-11-19 6:15 AM
SDI-12 doesn't seem to be very common because this question rarely came up here.
Maybe a version on Github that can be found here will help you further?
Regards
/Peter
2021-11-21 5:05 PM
int main(void)
{
/* USER CODE BEGIN 1 */
uint8_t UART1_rxBuffer[255] = {0};
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART1_UART_Init();
MX_I2C1_Init();
MX_SPI1_Init();
MX_USART2_UART_Init();
MX_USART3_UART_Init();
MX_DMA_Init();
MX_USART4_UART_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
HAL_UART_Transmit(&huart1, (uint8_t*)"Write Something\r\n", 17, HAL_MAX_DELAY);
while (1)
{
//HAL_UART_Receive(&huart1, &UART1_rxBuffer[0], 12, 500);
HAL_UART_Receive(&huart2, &UART1_rxBuffer[0], 12, 500);
HAL_UART_Transmit(&huart1, UART1_rxBuffer, strlen((char*)UART1_rxBuffer), HAL_MAX_DELAY);
UART1_rxBuffer[0] = 0;
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
static void MX_USART1_UART_Init(void)
{
/* USER CODE BEGIN USART1_Init 0 */
/* USER CODE END USART1_Init 0 */
/* USER CODE BEGIN USART1_Init 1 */
/* USER CODE END USART1_Init 1 */
huart1.Instance = USART1;
huart1.Init.BaudRate = 1200;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_UART_Init(&huart1) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&huart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&huart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&huart1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART1_Init 2 */
/* USER CODE END USART1_Init 2 */
}
static void MX_USART2_UART_Init(void)
{
/* USER CODE BEGIN USART2_Init 0 */
/* USER CODE END USART2_Init 0 */
/* USER CODE BEGIN USART2_Init 1 */
/* USER CODE END USART2_Init 1 */
huart2.Instance = USART2;
huart2.Init.BaudRate = 1200;
huart2.Init.WordLength = UART_WORDLENGTH_7B;
huart2.Init.StopBits = UART_STOPBITS_1;
huart2.Init.Parity = UART_PARITY_EVEN;
huart2.Init.Mode = UART_MODE_TX_RX;
huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart2.Init.OverSampling = UART_OVERSAMPLING_16;
huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_ENABLE;
huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1;
huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;
if (HAL_HalfDuplex_Init(&huart2) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetTxFifoThreshold(&huart2, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_SetRxFifoThreshold(&huart2, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK)
{
Error_Handler();
}
if (HAL_UARTEx_DisableFifoMode(&huart2) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN USART2_Init 2 */
/* USER CODE END USART2_Init 2 */
}Hi master,
This is my codes. Arduino always ping "0I!" every 1 sec.
while(1)
{
String command = "";
command += "0";
command += "I!";
Serial.println("Send: " + command);
mySDI12.sendCommand(command);
delay(1000);
}
2021-11-21 5:10 PM
Hi master,
Thanks for you suggestion. Share with me if there are new update added for SDI-12 example using STMcubeIDE
Regards
2021-11-21 5:18 PM
> huart1.Init.WordLength = UART_WORDLENGTH_8B;
> huart1.Init.StopBits = UART_STOPBITS_1;
> huart1.Init.Parity = UART_PARITY_NONE;
> huart1.Init.Mode = UART_MODE_TX_RX;
> huart2.Init.WordLength = UART_WORDLENGTH_7B;
> huart2.Init.StopBits = UART_STOPBITS_1;
> huart2.Init.Parity = UART_PARITY_EVEN
> huart2.Init.Mode = UART_MODE_TX_RX;
The code you posted uses two UARTs, neither of which is in single wire mode. One has 8 data bits and no parity, the other has 6 data bits plus one even parity. Hard to know what the intention is here.
2021-11-22 12:09 AM
.
2021-11-22 1:12 AM
.
2021-11-22 1:15 AM
uart 1 for debug, uart 2 for SDI-12 sir.. means uart 2 is for single wire. It shows in the init function as below.
if (HAL_HalfDuplex_Init(&huart2) != HAL_OK)
{
Error_Handler();
}Regards
2021-11-22 7:45 AM
You're right. The word length is still incorrect, however.