2024-08-28 4:45 AM
Hello All,
I wanted to copy two files from the STM32Cube directory to use arm_math.h, but those files are nowhere to be found.
・STM32Cube\Repository\STM32Cube_FW_F4_Vxxxx\Drivers\CMSIS\Lib\ARM\arm_cortexM4lf_math.lib
・STM32Cube\Repository\STM32Cube_FW_F4_Vxxxx\Drivers\CMSIS\Lib\GCC\libarm_cortexM4lf_math.a
What should we do when these two are not available?
best regards.
STM32F407vgt6,cubeIDE Version: 1.14.1,CMSIS Version5.9.0
Solved! Go to Solution.
2024-08-28 8:05 AM
@KDJEM.1 ,Thank you for your response.
The problem has not yet been resolved.
It is a little difficult to give you the entire project as it is because of all the things involved. We are really sorry.
best regards.
2024-08-28 8:18 AM
@baby_chicken wrote:It is a little difficult to give you the entire project as it is because of all the things involved. We are really sorry.
Create a minimum but complete project which demonstrates the issue, and share that.
In doing so, you might actually get a working project - which you could then compare to your real project to see what's different ...
2024-08-28 8:22 AM
@KDJEM.1 , is it possible to ask you to wait a little?
Thank you in advance.
2024-08-28 11:58 PM
Hi @baby_chicken ,
Sure, you are always welcome :).
If you want you can send a minimum project by Private Message.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-08-29 4:26 AM
Thank you so much @KDJEM.1 .
2024-08-30 12:05 AM - edited 2024-08-30 2:49 AM
@KDJEM.1 , this is a minimal project.
You may have thrown an error in minimizing the project.
Sorry, thank you for your cooperation.
2024-08-30 3:07 AM - edited 2024-08-30 3:08 AM
Hi @baby_chicken ,
Could you please add the ../Drivers/CMSIS_DSP/Include path and the ../Drivers/CMSIS_DSP/PrivateInclude path to "MCU G++ Compiler" "Include paths"
Thank you;
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.