2020-09-10 04:11 AM
I found links here:https://www.st.com/en/development-tools/stm32cubeide.html
but, it doesn't work.
Solved! Go to Solution.
2020-09-11 12:58 AM
Weird, I've been able to download the STM32CubeIDE Generic Linux Installer without troubles. This is actually my preferred one since it is the only installation procedure allowing self-update application. Other installation modes will stay on a fixed version. There are pros and cons to this depending on your needs.
The installation guide is under Resources / User Manuals / UM2563.
Once zip downloaded and extracted you get a .sh script file.
Make it executable (chmod +x ***.sh) and launch it from a terminal.
For Ubuntu, either:
sudo ./st-stm32cubeide_1.4.0_7511_20200720_0928_amd64.deb_bundle.sh
or
./st-stm32cubeide_1.4.0_7511_20200720_0928_amd64.sh
The 2nd will ask you later to execute some install steps as sudo. This is required since STLink-Server, Udev rules for STLink/Jlink installation need to change some basic system settings.
HTH 🙂
2020-09-10 04:29 AM
Hi MQi.1,
What exactly won't work ?
Reading your post it could be many things: the installer download, the installation guide document download, the installer itself, the installed application, etc...
Please provide us with more details about, like the error message and/or the way that conducted to this error.
2020-09-11 12:26 AM
When I selected "STM32CubeIDE Generic Linux Installer", I could downloaded nothing.
Then I downloaded "STM32CubeIDE Debian Linux Installer", I got a zip file, and I could extract it, then how to do next?
I tried to double click it, it just said"loading ...sh", is that OK, or I should input some codes like "sudo ..."?
2020-09-11 12:29 AM
I got this one:
st-stm32cubeide_1.4.0_7511_20200720_0928_amd64.deb_bundle.sh
How to do with it?
Is there a manual or tutorial for installing and running CubeIDE ON linux?
2020-09-11 12:58 AM
Weird, I've been able to download the STM32CubeIDE Generic Linux Installer without troubles. This is actually my preferred one since it is the only installation procedure allowing self-update application. Other installation modes will stay on a fixed version. There are pros and cons to this depending on your needs.
The installation guide is under Resources / User Manuals / UM2563.
Once zip downloaded and extracted you get a .sh script file.
Make it executable (chmod +x ***.sh) and launch it from a terminal.
For Ubuntu, either:
sudo ./st-stm32cubeide_1.4.0_7511_20200720_0928_amd64.deb_bundle.sh
or
./st-stm32cubeide_1.4.0_7511_20200720_0928_amd64.sh
The 2nd will ask you later to execute some install steps as sudo. This is required since STLink-Server, Udev rules for STLink/Jlink installation need to change some basic system settings.
HTH 🙂
2020-09-11 06:50 AM
Did you installed "Generic Linux" or "Debian Linux Installer"?
Why here is "deb": sudo ./st-stm32cubeide_1.4.0_7511_20200720_0928_amd64.deb_bundle.sh
2020-09-11 06:56 AM
I downloaded and installed "Generic Linux", and got these:
2020-09-11 07:02 AM
Quick answer is both.
"Debian Linux Installer" requires sudo on the command-line since calling the package manager (apt, dpkg) has to be done as admin.
STM32CubeIDE will be installed in /opt/st/, owned by root, and shared among all workstation users.
"Generic Linux" does not necessary requires sudo on the command-line. Don't use it to enable the self-update feature in STM32CubeIDE, this is how I usually install the tool.
STM32CubeIDE will be installed where you want, owned by you or root (sudo).
2020-09-11 07:04 AM
I do not see the .sh script, are you sure that you're not trying to execute the extracted folder from the zip archive.
Try cd en.st-stm32cubeide_1.4.0_7511_20200720_0928_amd64_sh first and do the chmod command on the .sh file.
2020-09-11 08:28 PM
I could only download "STM32CubeIDE Generic Linux Installer", since when I downloaded "STM32CubeIDE Debian Linux Installer", it would also sent me a link, but when I clicked the link, it prompted: