cancel
Showing results for 
Search instead for 
Did you mean: 

How to get CubeIDE version for MacOS 12.7 Monterey (Intel)

noName123
Associate

1. Which CubeIDE version is the latest that supports MacOS 12.7 Monterey for the Intel-based Macs?

2. Where do I go to download it?

Thanks

2 REPLIES 2
Ghofrane GSOURI
ST Employee

Hello @noName123 

 I recommend using the latest STM32CubeIDE 1.17.0, which supports the following operating systems and architectures:

  • Windows: Windows® 10 and 11 (64-bit)
  • Linux: Ubuntu® LTS 22.04, LTS 24.04, and Fedora® 40
  • macOS: macOS® 14 (Sonoma) and macOS® 15 (Sequoia)

Please note that while STM32CubeIDE may work on macOS 12.7, it is not officially supported on this version. Therefore, to ensure proper functionality on macOS 12.7, I recommend using a virtual machine (VM) with one of the supported operating systems listed above.

You can download the latest STM32CubeIDE from this LINK 

THX

Ghofrane

noName123
Associate

Thank you for your reply.

Do any earlier versions of CubeIDE support MacOS 12.7?

I've had bad experience using a virtual machine with other tools and would rather use an earlier version of CubeIDE if there is one that supports my OS.