2024-12-10 11:18 AM
1. Which CubeIDE version is the latest that supports MacOS 12.7 Monterey for the Intel-based Macs?
2. Where do I go to download it?
Thanks
2024-12-11 12:21 AM - edited 2024-12-11 04:22 AM
Hello @noName123
I recommend using the latest STM32CubeIDE 1.17.0, which supports the following operating systems and architectures:
Please note that while STM32CubeIDE may work on macOS 12.7, it is not officially supported on this version. Therefore, to ensure proper functionality on macOS 12.7, I recommend using a virtual machine (VM) with one of the supported operating systems listed above.
You can download the latest STM32CubeIDE from this LINK
THX
Ghofrane
2024-12-12 07:55 AM
Thank you for your reply.
Do any earlier versions of CubeIDE support MacOS 12.7?
I've had bad experience using a virtual machine with other tools and would rather use an earlier version of CubeIDE if there is one that supports my OS.