2020-06-03 11:12 AM
CubeIDE version 1.2.0
Cloning a git repo with a .ioc file in it, how to generate code?
When right clicking the "Generate code" is grayed out. The only method that has worked seems to be opening the .ioc file, toggling a checkbox to generate a change and then saving to cause code generation.
Is there a way to generate code when ever I want? or force the code generation even if there are no changes detected?
2020-06-14 12:37 PM
Sounds weird. Fact is code generation is only enable if Device Configuration Editor is opened (.ioc file edition on going in other words). But if Device Configuration Editor is active no need to get any change to get access and run code generation.
Sounds you're able to rely on Device Configuration Tool so ... ? Could you share some snapshot and/or your .ioc file ?
2023-07-16 01:32 PM
It doesn't matter if there is a need to do it or not. If customer wants, it must be provided. Just that simple.
2023-07-16 02:21 PM
I would like to carefully point out that this thread is already three years old and nothing has happened here since then, nor had the TO given any additional information.
In the meantime we are many, many versions further along with CubeIDE and such problems seem to have been eliminated.
Regards /Peter