2021-05-03 1:05 PM
2021-05-03 1:51 PM
Do you need seconds or also microseconds?
Is a number sufficient or should it be a text string?
I use a C++ class, but the code should work with C, too:
with
std::time_t t;
uint32_t microseconds;
For storage I convert time_t to uint32_t
I use this code:
/* we use mktime here
If you look at the code, it does not really look very clean and breaks some coding rules,
see https://code.woboq.org/userspace/glibc/time/mktime.c.html
but as it is used for 50 years now, we assume it is quite tested.
*/
RTC_TimeTypeDef ti;
RTC_DateTypeDef da;
(void) HAL_RTC_GetTime(&hrtc, &ti, RTC_FORMAT_BIN);
(void) HAL_RTC_GetDate(&hrtc, &da, RTC_FORMAT_BIN);
struct tm tim = {0};
tim.tm_hour = ti.Hours;
tim.tm_min = ti.Minutes;
tim.tm_sec = ti.Seconds;
tim.tm_year = da.Year+100;
tim.tm_mon = da.Month -1;
tim.tm_mday = da.Date;
tim.tm_isdst = 0;
if (ti.DayLightSaving == RTC_DAYLIGHTSAVING_SUB1H)
{
tim.tm_isdst = -1;
}
else if (ti.DayLightSaving == RTC_DAYLIGHTSAVING_ADD1H)
{
tim.tm_isdst = 1;
}
t = mktime(& tim);
/* HAL: Second fraction ratio * time_unit= [(SecondFraction-SubSeconds)/(SecondFraction+1)] * time_unit */
microseconds = 1000000 * (ti.SecondFraction - ti.SubSeconds) / (ti.SecondFraction + 1);
}
2021-05-03 2:52 PM
I need it in seconds, and a number is sufficient enough.
2021-05-03 2:57 PM
> Also, how to receive this timestamp?
Do you mean to write it back into RTC?
RTC_TimeTypeDef tTime;
RTC_DateTypeDef tDate;
std::tm * ptm = std::localtime(&t);
if (ptm)
{
tTime.Hours = uint8_t(ptm->tm_hour);
tTime.Minutes = uint8_t(ptm->tm_min);
tTime.Seconds = uint8_t(ptm->tm_sec);
//tTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
tTime.StoreOperation = RTC_STOREOPERATION_RESET;
if (HAL_RTC_SetTime(&hrtc, &tTime, RTC_FORMAT_BIN) != HAL_OK)
{
Error_Handler();
}
if (ptm->tm_wday == 0)
{
tDate.WeekDay = 7;
}
else
{
tDate.WeekDay =uint8_t(ptm->tm_wday);
}
// month oct to dec would be 0x10, 0x11, 0x12 according to STM but 10, 11, 12 can also be used
// the HAL_RTC_SetDate makes a conversion if required
tDate.Month = uint8_t(ptm->tm_mon) + 1;
tDate.Date = uint8_t(ptm->tm_mday);
// year is since 1900 in tm but since 2000 in HAL_RTC_SetDate
tDate.Year = uint8_t(ptm->tm_year+1900-2000);
if (ptm->tm_isdst == 1)
{
tTime.DayLightSaving = RTC_DAYLIGHTSAVING_ADD1H;
}
else if (ptm->tm_isdst == -1)
{
tTime.DayLightSaving = RTC_DAYLIGHTSAVING_SUB1H;
}
else
{
tTime.DayLightSaving = RTC_DAYLIGHTSAVING_NONE;
}
if (HAL_RTC_SetDate(&hrtc, &tDate, RTC_FORMAT_BIN) != HAL_OK)
{
Error_Handler();
}
HAL_RTCEx_BKUPWrite(&hrtc,RTC_BKP_DR0,0x32F2); // lock it in with the backup registers
}
2021-05-03 3:04 PM
Like for example, I would like to extract that RTC data when a button is pressed and stored that timestamp.
2021-05-03 9:27 PM
Which STM32?
Simply read RTC->TR followed by reading RTC->DR (unless you've set BYPSHD, in which case you don't need to read the date).
JW
2021-05-03 9:42 PM
2021-05-04 1:48 PM
uint32_t time, date;
time = RTC->TR; // reading TR locks
date = RTC->DR; // reading DR unlocks
I don't use the 'WB55.
JW