2022-04-07 5:33 PM
Where can I download an archive of the GNU Tools for STM32 separate from the STM32Cube IDE?
Alternatively where can I find your open-sourced patches that you list in the information center?
2022-04-12 9:18 AM
@Markus GIRDLAND Since you commented on the related thread "What are the GNU Tools for STM32 patches ..." a while ago, can you speak to my question? Or maybe @mattias norlander ?
Ideally, the GNU Tools for STM32 patches and releases with binary archives would be made available via another repo on the https://github.com/STMicroelectronics organization. Don't the open-source licenses obligate you to make the patches available?
2022-04-12 4:28 PM
@Bryce SchoberThe Toolchain manager widget of CubeIDE can discover and download toolchains released after CubeIDE releases, both ST and ARM versions.
So these toolchain packages are already available online...
2022-04-12 11:31 PM
Hi Bryce,
As Pavel mentioned, toolchains are available via toolchain manager. If you really the toolchain in a zip-file I suppose we can provide some specific zip-file in a file share. Drop me your e-mail address in PM, the one on you profile does not work. Which OS?
2022-07-12 5:06 AM
I wonder is there a specific reason why toolchains could not just be available under the "Software Development Tools" section?
There are some valid use cases for stand-alone toolchains. For example, when developing an application in Cube IDE, and also wanting to use exactly the same toolchain in CI/CD system. Bundling the entire CubeIDE to run it in headless mode is "little" excessive.
2022-07-12 5:56 AM
A good idea. Would be useful for restrictive environments where CubeIDE cannot go to the web and download stuff. Even thru a proxy.
2022-12-13 4:09 AM
Hi there,
Is there any news about this?
2023-05-15 9:37 AM
This is a great idea!
The Toolchain Manager is a awesome feature but it is slow to launch and update. Our projects are not using the current default toolchain. A simple way to download the same GNU Tools for STM32 binaries would be great to get them on the CI/CD system, and also to speed up installing the dev environment for new developers.
2023-05-16 10:51 AM
Just by way of followup, ST now offers the STM32CubeCLT, described as "an all-in-one multi-OS command-line toolset, which is part of the STM32Cube ecosystem".
As with all ST packages, it's kinda annoyingly wrapped in a .zip file, but it seems like it might fulfill my basic desires at the time, which are:
2023-08-14 11:52 AM
I am also looking for a way to use an older toolchain within a custom docker image for CI/CD. Has there been any further information on downloadable toolchains outside of the Toolchain Manager?