cancel
Showing results for 
Search instead for 
Did you mean: 

how to customize debug perspective in stm32cubeide?

JG
Associate III

0693W00000GWowIQAT.pngHi, I would like to customize the debug perspective but I can't remove the selected windows. I want to remove the window with the red box to leave the main.c file in the entire horizontal space, but it is associated with the editor in C ++ perspective. I also want to remove the green box window which is practically useless. I welcome suggestions in this regard.

1 ACCEPTED SOLUTION

Accepted Solutions
Julien D
ST Employee

Hi @Juan Gómez​ 

Seems to be possible with the following steps.

Hope this helps

View solution in original post

8 REPLIES 8
Chloe Meunier
ST Employee

Hello,

did you try to manage these view in Window -- > Show View ?

JG
Associate III

Hi, I did but they are not windows with specific functionalities. They are something like modules/windows of the Debug perspective.

I tried too with Window -> Properties -> Run Debug -> Perspectives ,but when switch of run to debug, the window in the red box load again the .c file

Julien D
ST Employee

Hi @Juan Gómez​ 

Seems to be possible with the following steps.

Hope this helps

JG
Associate III

It works, thanks a lot @Julien D_OEHAUDT​ !!

Great! Don't hesitate to flag this topic as "Answered" ;)

JG
Associate III

Ok, sure :thumbs_up: !!

JG
Associate III

I think it is done, I appreciate if it's possible to verify.

You did it perfectly, thanks :thumbs_up: