2021-10-03 3:46 PM
1) I added to folder Core/Inc file my_lib.h
2) Added to folder Core/Src file my_lib.cpp
3) I added #include "my_lib.cpp" to main.cpp
In tmy_lib.cpp I have only one class for testing. This class works with PWM.
When I compile project I get errors that such names are not found:
TIM_Channel_1, htim, uint32_t, so on...
So, it seems that this my_lib.h is compiled first and before default libraries goted by CubeMX. How to solve this problem and to compile added file at the end of the project?
Solved! Go to Solution.
2021-10-04 6:05 AM
OK, problem was solved.
I was wrong in syntax of classes in additional files. Now everything works fine.
2021-10-03 4:05 PM
Don't #include source files from other source files. That's now how C or C++ is intended to work.
At the beginning of files that use HAL, #include "stm32f4xx_hal.h" or similar. Don't #include any other HAL files.
2021-10-04 1:15 AM
Thank you for your answer, it's helped a little. But may be I'm doint something wrong.
I got error "undefined reference to class:
c:\st\stm32cubeide_1.7.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: E:/STM/les_4_4_PWM_output/Debug/../Core/Src/main.cpp:177: undefined reference to `PWM::PWM()'
c:\st\stm32cubeide_1.7.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: E:/STM/les_4_4_PWM_output/Debug/../Core/Src/main.cpp:177: undefined reference to `PWM::PWM()'
c:\st\stm32cubeide_1.7.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: E:/STM/les_4_4_PWM_output/Debug/../Core/Src/main.cpp:177: undefined reference to `PWM::PWM()'
c:\st\stm32cubeide_1.7.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: E:/STM/les_4_4_PWM_output/Debug/../Core/Src/main.cpp:193: undefined reference to `PWM::SoftBlink(TIM_HandleTypeDef*, unsigned long, int, unsigned long)'
c:\st\stm32cubeide_1.7.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: E:/STM/les_4_4_PWM_output/Debug/../Core/Src/main.cpp:194: undefined reference to `PWM::SoftBlink(TIM_HandleTypeDef*, unsigned long, int, unsigned long)'
c:\st\stm32cubeide_1.7.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: E:/STM/les_4_4_PWM_output/Debug/../Core/Src/main.cpp:195: undefined reference to `PWM::SoftBlink(TIM_HandleTypeDef*, unsigned long, int, unsigned long)'
c:\st\stm32cubeide_1.7.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_2.0.0.202105311346\tools\arm-none-eabi\bin\ld.exe: E:/STM/les_4_4_PWM_output/Debug/../Core/Src/main.cpp:196: undefined reference to `PWM::SoftBlink(TIM_HandleTypeDef*, unsigned long, int, unsigned long)'
collect2.exe: error: ld returned 1 exit status
I have added such .h file Core/Inc/mypwm.h
#ifndef INC_MYPWM_H_
#define INC_MYPWM_H_
#include "stm32f3xx_hal.h"
class PWM {
protected:
int32_t ch_dir;
private:
uint32_t CH_DC;
public:
PWM();
void SoftBlink(TIM_HandleTypeDef *htim, uint32_t Channel, int step, uint32_t max_ARR);
}; // end class
#endif /* INC_MYPWM_H_ */
and Core/Src/mypwm.cpp is:
#include "stm32f3xx_hal.h"
#include "assert.h"
class PWM {
protected:
int32_t ch_dir; // =1 - increase pwm, -1 - decreese pwm
private:
uint32_t CH_DC; // max Auto Reload Register (ARR)
public:
PWM() // кон�?труктор за умовчуванн�?м
{
ch_dir=1;
CH_DC=0;
}
void SoftBlink(TIM_HandleTypeDef *htim, uint32_t Channel, int step, uint32_t max_ARR){
while ((CH_DC < max_ARR) & (ch_dir >=0)) {
switch (Channel){
case TIM_CHANNEL_1 : {
htim->Instance->CCR1 = CH_DC;
break;
}
case TIM_CHANNEL_2 : {
htim->Instance->CCR2 = CH_DC;
break;
}
case TIM_CHANNEL_3 : {
htim->Instance->CCR3 = CH_DC;
break;
}
case TIM_CHANNEL_4 : {
htim->Instance->CCR4 = CH_DC;
break;
}
default :
assert(0);
} // end_switch
CH_DC += step;
HAL_Delay(1);
} // end_while
while ((CH_DC > 0) & (ch_dir <0)) {
switch (Channel){
case TIM_CHANNEL_1 : {
htim->Instance->CCR1 = CH_DC;
break;
}
case TIM_CHANNEL_2 : {
htim->Instance->CCR2 = CH_DC;
break;
}
case TIM_CHANNEL_3 : {
htim->Instance->CCR3 = CH_DC;
break;
}
case TIM_CHANNEL_4 : {
htim->Instance->CCR4 = CH_DC;
break;
}
} // end_switch
CH_DC -=step;
HAL_Delay(1);
} // end_while
if (ch_dir>=0) {
ch_dir =-1;
}
else {
ch_dir=1;
}
} //end SoftBlink
}; // end class
I don't anderstand what I'm doing wrong.
In the main.cpp I make
#include "mypwm.h"
2021-10-04 6:05 AM
OK, problem was solved.
I was wrong in syntax of classes in additional files. Now everything works fine.
2021-10-04 6:13 AM
Make sure mypwm.cpp is being compiled. Look in the build log.
Try to right click the project and clean/refresh.