2020-10-05 5:59 AM
I have just downloaded the STM32 IDE, and I find it very complicated to use it. I am using a bare MCU, no dev board, hence I am using the STLink-V2 to program the MCU. I want some help on how to write my program to blink an led and set up the STLink-V2 to run with the CubeIDE.
Thank you
2020-10-05 6:09 AM
Perhaps there are some video tutorials you could watch?
Writing a blinky program on a NUCLEO vs Custom + ST-LINK should be materially similar. You'd need to know the IC you're using, and the pin the LED is attached too.
Perhaps find an example or template project which are a close match, and start from there.
2020-10-05 6:58 AM
Otherwise, you can follow our Wiki STM32 MCU here below, step #1, #2 and #3.
https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:STM32_step_by_step_overview
BR
rrom
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2020-10-05 8:31 PM
Thank you I am using a STM32F030R8, I have followed some, but when I connect my ST-Link V2 to my computer it says"Error in initialising ST-Link device" "Error with command: gdb --version" what am I supposed to do?