2020-08-10 11:01 AM
How do I rename (proper way) an STM32 project?
If I press F2 I can rename the name of the project, but the project folder still have the same name. If I change the name of the folder, then I get errors.
Why?
Is there a proper way to rename a project?
I'm using STM32CubeIDE 1.3.0.
Solved! Go to Solution.
2020-08-10 12:28 PM
Don't know if that's the proper way, but if you rename (F2) in STM32cubeIDE first, delete the project form workspace (but not from file system ;-), rename the folder and open the project in the renamed folder again, it will be re-added to the workspace and you have completed the task, i.e. no more errors. Existing Debug/Run configurations must be renamed separtely.
2020-08-10 12:28 PM
Don't know if that's the proper way, but if you rename (F2) in STM32cubeIDE first, delete the project form workspace (but not from file system ;-), rename the folder and open the project in the renamed folder again, it will be re-added to the workspace and you have completed the task, i.e. no more errors. Existing Debug/Run configurations must be renamed separtely.
2020-08-10 2:39 PM
It works!
2024-09-14 12:18 PM
@KnarfB wrote:Existing Debug/Run configurations must be renamed separtely.
What do you mean? And how you do that?
Thank you