2022-10-16 01:56 PM
After Pasting one Project, and allowing Uptading Reference Button, I tried to open the *ioc file which issued "error". Then, I had to rename to the newest Project name, then I was abble to open the *.ioc file. So, I might ask: Is it the correct "project copy" task? Doesn't the CUBE aren't able to fix all the newest references, based on the newest copied file name? Regards.
2022-10-16 04:51 PM
This is not in the known issues for v1.10.1
https://wiki.st.com/stm32mcu/wiki/STM32CubeIDE:STM32CubeIDE_errata_1.10.x#Known_issues
Just copy (and rename) the project in the simplest way that works, and report a bug if you like to.
2022-10-16 05:22 PM
Follows my CUBE's version->
Version: 1.10.1
Build: 12716_20220707_0928 (UTC)
(C) 2022 STMicroelectronics ALL RIGHTS RESERVED
2022-10-17 03:07 AM
Hello @JSILV.2
First let me thank you for posting.
I tried to copy a project and simply rename it as @Pavel A. mentioned. And this is what I found:
If this didn't solve the issue you have; could you, please describe in detail the steps you did so I am able the use case.
Kind regards,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-10-17 03:45 PM
Dear Cherni.
The so called issue works as you just described. My conclusion is exact as you instructed me. Therefore, I made the best wayout.
Regards.