2022-05-03 12:03 PM
I notice that the I2C1 setup in the IDE is different than the I2C2 setup. I will try I2C1 to see if it can work, but how would I get I2C2 working?
2022-05-03 1:16 PM
Well options there are that whatever else is attached to the bus is clamping them, or not in I2C mode (perhaps some SPI/I2C mode device), or that PA9/PA10 are in some initialized state (USART1) and conflicting with the settings on PA11/PA12
Check all your GPIO pin settings in code, and at register level.
Disconnect other portions of the circuit.
Check for shorts.
Perhaps check driving the GPIOs directly.