‎2021-11-07 10:31 AM
make -j4 all
arm-none-eabi-gcc "../Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal.c" -mcpu=cortex-m0 -std=gnu11 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32F072xB -c -I../Core/Inc -I../Drivers/STM32F0xx_HAL_Driver/Inc -I../Drivers/STM32F0xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32F0xx/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal.d" -MT"Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal.o" --specs=nano.specs -mfloat-abi=soft -mthumb -o "Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal.o"
arm-none-eabi-gcc "../Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_adc.c" -mcpu=cortex-m0 -std=gnu11 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32F072xB -c -I../Core/Inc -I../Drivers/STM32F0xx_HAL_Driver/Inc -I../Drivers/STM32F0xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32F0xx/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_adc.d" -MT"Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_adc.o" --specs=nano.specs -mfloat-abi=soft -mthumb -o "Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_adc.o"
arm-none-eabi-gcc "../Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_adc_ex.c" -mcpu=cortex-m0 -std=gnu11 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32F072xB -c -I../Core/Inc -I../Drivers/STM32F0xx_HAL_Driver/Inc -I../Drivers/STM32F0xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32F0xx/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_adc_ex.d" -MT"Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_adc_ex.o" --specs=nano.specs -mfloat-abi=soft -mthumb -o "Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_adc_ex.o"
arm-none-eabi-gcc "../Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_can.c" -mcpu=cortex-m0 -std=gnu11 -g3 -DDEBUG -DUSE_HAL_DRIVER -DSTM32F072xB -c -I../Core/Inc -I../Drivers/STM32F0xx_HAL_Driver/Inc -I../Drivers/STM32F0xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Device/ST/STM32F0xx/Include -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_can.d" -MT"Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_can.o" --specs=nano.specs -mfloat-abi=soft -mthumb -o "Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_can.o"
In file included from ../Drivers/CMSIS/Device/ST/STM32F0xx/Include/stm32f0xx.h:149,
from ../Drivers/STM32F0xx_HAL_Driver/Inc/stm32f0xx_hal_def.h:30,
from ../Drivers/STM32F0xx_HAL_Driver/Inc/stm32f0xx_hal_rcc.h:29,
from ../Core/Inc/stm32f0xx_hal_conf.h:192,
from ../Drivers/STM32F0xx_HAL_Driver/Inc/stm32f0xx_hal.h:30,
from ../Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal.c:36:
../Drivers/CMSIS/Device/ST/STM32F0xx/Include/stm32f072xb.h:116:10: fatal error: core_cm0.h: No such file or directory
116 | #include "core_cm0.h" /* Cortex-M0 processor and core peripherals */
| ^~~~~~~~~~~~
compilation terminated.
In file included from ../Drivers/CMSIS/Device/ST/STM32F0xx/Include/stm32f0xx.h:149,
from ../Drivers/STM32F0xx_HAL_Driver/Inc/stm32f0xx_hal_def.h:30,
from ../Drivers/STM32F0xx_HAL_Driver/Inc/stm32f0xx_hal_rcc.h:29,
from ../Core/Inc/stm32f0xx_hal_conf.h:192,
from ../Drivers/STM32F0xx_HAL_Driver/Inc/stm32f0xx_hal.h:30,
from ../Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_adc_ex.c:34:
../Drivers/CMSIS/Device/ST/STM32F0xx/Include/stm32f072xb.h:116:10: fatal error: core_cm0.h: No such file or directory
116 | #include "core_cm0.h" /* Cortex-M0 processor and core peripherals */
| ^~~~~~~~~~~~
compilation terminated.
make: *** [Drivers/STM32F0xx_HAL_Driver/Src/subdir.mk:76: Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal.o] Error 1
make: *** Waiting for unfinished jobs....
make: *** [Drivers/STM32F0xx_HAL_Driver/Src/subdir.mk:76: Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_adc_ex.o] Error 1
In file included from ../Drivers/CMSIS/Device/ST/STM32F0xx/Include/stm32f0xx.h:149,
from ../Drivers/STM32F0xx_HAL_Driver/Inc/stm32f0xx_hal_def.h:30,
from ../Drivers/STM32F0xx_HAL_Driver/Inc/stm32f0xx_hal_rcc.h:29,
from ../Core/Inc/stm32f0xx_hal_conf.h:192,
from ../Drivers/STM32F0xx_HAL_Driver/Inc/stm32f0xx_hal.h:30,
from ../Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_can.c:213:
../Drivers/CMSIS/Device/ST/STM32F0xx/Include/stm32f072xb.h:116:10: fatal error: core_cm0.h: No such file or directory
116 | #include "core_cm0.h" /* Cortex-M0 processor and core peripherals */
| ^~~~~~~~~~~~
compilation terminated.
In file included from ../Drivers/CMSIS/Device/ST/STM32F0xx/Include/stm32f0xx.h:149,
from ../Drivers/STM32F0xx_HAL_Driver/Inc/stm32f0xx_hal_def.h:30,
from ../Drivers/STM32F0xx_HAL_Driver/Inc/stm32f0xx_hal_rcc.h:29,
from ../Core/Inc/stm32f0xx_hal_conf.h:192,
from ../Drivers/STM32F0xx_HAL_Driver/Inc/stm32f0xx_hal.h:30,
from ../Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_adc.c:303:
../Drivers/CMSIS/Device/ST/STM32F0xx/Include/stm32f072xb.h:116:10: fatal error: core_cm0.h: No such file or directory
116 | #include "core_cm0.h" /* Cortex-M0 processor and core peripherals */
| ^~~~~~~~~~~~
compilation terminated.
make: *** [Drivers/STM32F0xx_HAL_Driver/Src/subdir.mk:76: Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_can.o] Error 1
make: *** [Drivers/STM32F0xx_HAL_Driver/Src/subdir.mk:76: Drivers/STM32F0xx_HAL_Driver/Src/stm32f0xx_hal_adc.o] Error 1
"make -j4 all" terminated with exit code 2. Build might be incomplete.
‎2021-11-07 12:04 PM
> ../Drivers/CMSIS/Device/ST/STM32F0xx/Include/stm32f072xb.h:116:10: fatal error: core_cm0.h: No such file or directory
It says it can't find core_cm0.h. Does it exist in your project? It should be at Drivers/CMSIS/Include/core_cm0.h. If not, regenerate the code or copy it from another project. Other files may also be missing.
If it does exist, ensure the include directories are set up to find it.
‎2021-11-07 12:12 PM
Ive observed that Cube does not generate the "normal files" by that i mean all core and header files like adc.c/adc.h as it used to do.
‎2021-11-07 12:13 PM
Also reinstalling cube does not help 😂
‎2021-11-07 12:18 PM
That didn't answer my question.
If you want separate files for each peripheral, you need to select that option in CubeMX, but that's a different problem than what you asked in the post.
Project Manager -> Code Generator -> Generated files -> Generate peripheral initialization as a pair of...
‎2021-11-07 12:22 PM
is your project in the project folder of the Repository that you are using ?
Find the file that's missing, I use Ultrasearch for that.
add the missing folder to the include folders, then recompile.
Which IDE is it ?
‎2021-11-07 12:25 PM
It is in the same folder. I added the missing file but the IDE does not seem to care.
STM32CubeIDE 1.7.0