2019-05-29 08:32 AM
I am unable to debug a simple blinky program created using the CubeMX software. The board I am using is a Nucleo F103RB board. The IDE seems to be able to flash the MCU but then I get a
ST-LINK SN : 0670FF363732594D43214619
ST-LINK FW : V2J34M25
Voltage : 3.26V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x410
Device name : STM32F101/F102/F103 Medium-density
Flash size : 128 KBytes
Device type : MCU
Device CPU : Cortex-M3
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a01408.srec
File : ST-LINK_GDB_server_a01408.srec
Size : 96 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sector 0
Download in Progress:
File download complete
Time elapsed during download operation: 00:00:00.477
Verifying ...
Download verified successfully
Error! Failed to read target status
Debugger connection lost.
Shutting down...
followed by this:
No source available for "(gdb[13].proc[42000].threadGroup[i1],gdb[13].proc[42000].OSthread[1]).thread[1].frame[0]"
The same project debugs fine using the TrueStudio IDE.
2019-06-20 01:14 PM
Hi Ankit,
I had the same issue with a imported atollic studio project. The reason was that the startup-file was excluded from build (right-click on the folder and select properties, go to the item 'C/C++ Build' and uncheck the box 'Exclude resource from build'. That solved the problem for me.
Hope this helps...
2019-06-21 04:45 AM
Hi Christian,
I just checked to make sure but the startup file & folder aren't excluded from the build in my case. I have tried importing TrueStudio projects created using the stand-alone version of CubeMX as well as new projects created using the inbuilt CubeMX plugin within the CubeIDE. No joy. I guess I'll have to continue using CubeMX+TrueSTUDIO 9.3 for now until ST fixes this :(