2022-01-18 9:57 AM
2022-01-18 11:04 PM
All IDEs is u nlimited, but comercial need pay for it.
STM32CubeIDE use gcc and this is unlimited...
2022-01-18 10:12 AM
Yes
2022-01-18 10:28 AM
What is the limit? Is there any other IDE that has an unlimited code size?
2022-01-18 11:04 PM
All IDEs is u nlimited, but comercial need pay for it.
STM32CubeIDE use gcc and this is unlimited...
2022-01-19 12:39 AM
Hello @AE104 ,
I would recommend you to use STM32CubeIDE, it is a free and based on the Eclipse framework and GCC toolchain for the development, and GDB for the debugging.
You can use STM32CubeIDE for all STM32 MCU or MPU, and without limited code size.
If a post answers your question, please select it as Best so that this thread will marked as solved.
Thanks
Imen
2022-01-21 2:15 PM
Thank you for your responses @Imen DAHMEN and @MM..1 !
I will try it.