HardFault occurs when initializing IwIP in NUCLEO-F429ZI.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-08 7:23 PM
HardFault occurs when initializing IwIP in NUCLEO-F429ZI.
LwIP is being tested using STM Nucleo-F429ZI Board.
I am using STM32CudeIDE Version 1.6.1 and an error occurs in FreeRTOS environment.
IPv4 DCHP is not used and IP Address Setting has been made.
/**
* LwIP initialization function
*/
void MX_LWIP_Init(void)
{
/* IP addresses initialization */
IP_ADDRESS[0] = 192;
IP_ADDRESS[1] = 168;
IP_ADDRESS[2] = 1;
IP_ADDRESS[3] = 10;
NETMASK_ADDRESS[0] = 255;
NETMASK_ADDRESS[1] = 255;
NETMASK_ADDRESS[2] = 255;
NETMASK_ADDRESS[3] = 0;
GATEWAY_ADDRESS[0] = 192;
GATEWAY_ADDRESS[1] = 168;
GATEWAY_ADDRESS[2] = 1;
GATEWAY_ADDRESS[3] = 1;
/* Initilialize the LwIP stack with RTOS */
tcpip_init( NULL, NULL );
/* IP addresses initialization without DHCP (IPv4) */
IP4_ADDR(&ipaddr, IP_ADDRESS[0], IP_ADDRESS[1], IP_ADDRESS[2], IP_ADDRESS[3]);
IP4_ADDR(&netmask, NETMASK_ADDRESS[0], NETMASK_ADDRESS[1] , NETMASK_ADDRESS[2], NETMASK_ADDRESS[3]);
IP4_ADDR(&gw, GATEWAY_ADDRESS[0], GATEWAY_ADDRESS[1], GATEWAY_ADDRESS[2], GATEWAY_ADDRESS[3]);
/* add the network interface (IPv4/IPv6) with RTOS */
netif_add(&gnetif, &ipaddr, &netmask, &gw, NULL, ðernetif_init, &tcpip_input);
/* Registers the default network interface */
netif_set_default(&gnetif);
if (netif_is_link_up(&gnetif))
{
/* When the netif is fully configured this function must be called */
netif_set_up(&gnetif);
}
else
{
/* When the netif link is down this function must be called */
netif_set_down(&gnetif);
}
/* USER CODE BEGIN 3 */
/* USER CODE END 3 */
}
Error Modules is
void udp_init(void)
{
#ifdef LWIP_RAND
udp_port = UDP_ENSURE_LOCAL_PORT_RANGE(LWIP_RAND());
#endif /* LWIP_RAND */
}
�?� 함수를 실행하면 HardFault_Handler()가 호출�?�니다.
void HardFault_Handler(void)
{
/* USER CODE BEGIN HardFault_IRQn 0 */
/* USER CODE END HardFault_IRQn 0 */
while (1)
{
/* USER CODE BEGIN W1_HardFault_IRQn 0 */
/* USER CODE END W1_HardFault_IRQn 0 */
}
}
It doesn't go any further here. If it is a bug, please tell me how to fix it.
Thank you.
- Labels:
-
Ethernet
-
FreeRTOS
-
STM32CubeIDE
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-08 8:05 PM
Have you tried debugging? Where does the hard fault occures?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-04-21 5:29 AM
Hello @Bhong.1​ ,
Could you please share your example zip for further check ?
Thanks in advance.
Walid.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-08-31 5:18 PM
Error Line Debug
mX_LWIP_Init(void)
{
void MX_LWIP_Init(void)
{
/* IP addresses initialization */
IP_ADDRESS[0] = 192;
IP_ADDRESS[1] = 168;
IP_ADDRESS[2] = 0;
IP_ADDRESS[3] = 81;
NETMASK_ADDRESS[0] = 255;
NETMASK_ADDRESS[1] = 255;
NETMASK_ADDRESS[2] = 255;
NETMASK_ADDRESS[3] = 0;
GATEWAY_ADDRESS[0] = 192;
GATEWAY_ADDRESS[1] = 168;
GATEWAY_ADDRESS[2] = 0;
GATEWAY_ADDRESS[3] = 254;
/* Initilialize the LwIP stack with RTOS */
tcpip_init( NULL, NULL ); -> Error This Line
tcpio.c file
tcpip_init(tcpip_init_done_fn initfunc, void *arg)
{
lwip_init(); ---> Error This Line
tcpip_init_done = initfunc;
tcpip_init_done_arg = arg;
if (sys_mbox_new(&tcpip_mbox, TCPIP_MBOX_SIZE) != ERR_OK) {
LWIP_ASSERT("failed to create tcpip_thread mbox", 0);
}
#if LWIP_TCPIP_CORE_LOCKING
if (sys_mutex_new(&lock_tcpip_core) != ERR_OK) {
LWIP_ASSERT("failed to create lock_tcpip_core", 0);
}
#endif /* LWIP_TCPIP_CORE_LOCKING */
sys_thread_new(TCPIP_THREAD_NAME, tcpip_thread, NULL, TCPIP_THREAD_STACKSIZE, TCPIP_THREAD_PRIO);
}
lwip/src/core/init.c
void
lwip_init(void)
{
#ifndef LWIP_SKIP_CONST_CHECK
int a = 0;
LWIP_UNUSED_ARG(a);
LWIP_ASSERT("LWIP_CONST_CAST not implemented correctly. Check your lwIP port.", LWIP_CONST_CAST(void *, &a) == &a);
#endif
#ifndef LWIP_SKIP_PACKING_CHECK
LWIP_ASSERT("Struct packing not implemented correctly. Check your lwIP port.", sizeof(struct packed_struct_test) == PACKED_STRUCT_TEST_EXPECTED_SIZE);
#endif
/* Modules initialization */
stats_init();
#if !NO_SYS
sys_init();
#endif /* !NO_SYS */
mem_init();
memp_init();
pbuf_init();
netif_init();
#if LWIP_IPV4
ip_init();
#if LWIP_ARP
etharp_init();
#endif /* LWIP_ARP */
#endif /* LWIP_IPV4 */
#if LWIP_RAW
raw_init();
#endif /* LWIP_RAW */
#if LWIP_UDP
udp_init();
#endif /* LWIP_UDP */
#if LWIP_TCP
tcp_init(); -> Error this point to
stm32f4xx_it.c file
void HardFault_Handler(void)
{
/* USER CODE BEGIN HardFault_IRQn 0 */
/* USER CODE END HardFault_IRQn 0 */
while (1)
{
/* USER CODE BEGIN W1_HardFault_IRQn 0 */
/* USER CODE END W1_HardFault_IRQn 0 */
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-08-31 6:29 PM
Have an effective Hard Fault Handler that can output actionable data so you can see the faulting instructions and registers
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
‎2021-08-31 7:09 PM
tcp_init(void)
{
#ifdef LWIP_RAND
tcp_port = TCP_ENSURE_LOCAL_PORT_RANGE(LWIP_RAND()); -> Error This Line
#endif /* LWIP_RAND */
}
Hardfault Like This..
Help me.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-07-10 12:10 PM
I am debugging an example from STM32H7-LwIP-Examples/STM32H745_Nucleo_M4_ETH at main · stm32-hotspot/STM32H7-LwIP-Examples · GitHub, However, it runs into HardFault_Handler at the following line in function udp_init:
UDP_ENSURE_LOCAL_PORT_RANGE(LWIP_RAND());
It crashes on the invocation of the "rand" function from stdlib !!!!!