cancel
Showing results for 
Search instead for 
Did you mean: 

Hardfault in NonSecure_Init

Riya
Associate II

 

 

#define VTOR_TABLE_NS_START_ADDR 0x08100000UL static void NonSecure_Init(void); static void MX_GPIO_Init(void); static void MX_GTZC_S_Init(void); static void MX_ICACHE_Init(void); int main(void) { HAL_Init(); /* GTZC initialisation */ MX_GTZC_S_Init(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_ICACHE_Init(); /* USER CODE BEGIN 2 */ /* USER CODE END 2 */ /*************** Setup and jump to non-secure *******************************/ NonSecure_Init(); while (1) { } } static void NonSecure_Init(void) { funcptr_NS NonSecure_ResetHandler; SCB_NS->VTOR = VTOR_TABLE_NS_START_ADDR; /* Set non-secure main stack (MSP_NS) */ __TZ_set_MSP_NS((*(uint32_t *)VTOR_TABLE_NS_START_ADDR)); /* Get non-secure reset handler */ NonSecure_ResetHandler = (funcptr_NS)(*((uint32_t *)((VTOR_TABLE_NS_START_ADDR) + 4U))); /* Start non-secure state software application */ NonSecure_ResetHandler(); } static void MX_GTZC_S_Init(void) { MPCBB_ConfigTypeDef MPCBB_Area_Desc = {0}; /* USER CODE BEGIN GTZC_S_Init 1 */ /* USER CODE END GTZC_S_Init 1 */ if (HAL_GTZC_TZSC_ConfigPeriphAttributes(GTZC_PERIPH_USART3, GTZC_TZSC_PERIPH_SEC|GTZC_TZSC_PERIPH_NPRIV) != HAL_OK) { Error_Handler(); } if (HAL_GTZC_TZSC_ConfigPeriphAttributes(GTZC_PERIPH_UCPD1, GTZC_TZSC_PERIPH_SEC|GTZC_TZSC_PERIPH_NPRIV) != HAL_OK) { Error_Handler(); } if (HAL_GTZC_TZSC_ConfigPeriphAttributes(GTZC_PERIPH_USB, GTZC_TZSC_PERIPH_SEC|GTZC_TZSC_PERIPH_NPRIV) != HAL_OK) { Error_Handler(); } if (HAL_GTZC_TZSC_ConfigPeriphAttributes(GTZC_PERIPH_LPUART1, GTZC_TZSC_PERIPH_SEC|GTZC_TZSC_PERIPH_NPRIV) != HAL_OK) { Error_Handler(); } if (HAL_GTZC_TZSC_ConfigPeriphAttributes(GTZC_PERIPH_I2C3, GTZC_TZSC_PERIPH_SEC|GTZC_TZSC_PERIPH_NPRIV) != HAL_OK) { Error_Handler(); } if (HAL_GTZC_TZSC_ConfigPeriphAttributes(GTZC_PERIPH_ETHERNET, GTZC_TZSC_PERIPH_SEC|GTZC_TZSC_PERIPH_NPRIV) != HAL_OK) { Error_Handler(); } if (HAL_GTZC_TZSC_ConfigPeriphAttributes(GTZC_PERIPH_ADC12, GTZC_TZSC_PERIPH_SEC|GTZC_TZSC_PERIPH_NPRIV) != HAL_OK) { Error_Handler(); } MPCBB_Area_Desc.SecureRWIllegalMode = GTZC_MPCBB_SRWILADIS_ENABLE; MPCBB_Area_Desc.InvertSecureState = GTZC_MPCBB_INVSECSTATE_NOT_INVERTED; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[0] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[1] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[2] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[3] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[4] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[5] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[6] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[7] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[8] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[9] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[10] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[11] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[12] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[13] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[14] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[15] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[16] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[17] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[18] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_SecConfig_array[19] = 0x00000000; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[0] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[1] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[2] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[3] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[4] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[5] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[6] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[7] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[8] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[9] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[10] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[11] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[12] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[13] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[14] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[15] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[16] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[17] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[18] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_PrivConfig_array[19] = 0xFFFFFFFF; MPCBB_Area_Desc.AttributeConfig.MPCBB_LockConfig_array[0] = 0x00000000; if (HAL_GTZC_MPCBB_ConfigMem(SRAM3_BASE, &MPCBB_Area_Desc) != HAL_OK) { Error_Handler(); } }
View more

 

 

Hi

I am trying to launch debug for TrustZone enabled setup but when NonSecure_Init() function hit in secure region instead of jumping into Nonsecure region . it's giving hardfault handler.

Also can I know what are the configuration settings to be done in STM32CubeProgrammer for my application to run in both secure and non secure correctly.

I suspect the issue seems to be because of settings in STM32cubeprogrammer.

Can anyone help me configure correct memory allocation and settings to be done for TrustZone enaled secure-NonSecure to work without trouble.

Thank You.

Riya_0-1712138637083.pngRiya_1-1712138679394.png

Riya_2-1712138700909.png

 

1 ACCEPTED SOLUTION

Accepted Solutions
Rim LANDOLSI
ST Employee

Hello @Riya  and welcome to the community,

 

The problem of the NonSecure_Init() function hitting the secure region instead of jumping to the non-secure region is due to improper memory allocation of secure and non-secure.
According to your configuration, it looks like both your banks are configured as secure. Try to change this:


SECWM2_START value = 0x01

SECWM2_END value = 0x00

apply and save and try to debug.


Check your jump address in the secure firmware, it should be the start of your bank 2 address 0x08100000UL, which is not the case as your CubeProgrammer configuration is for bank 2.

Hope this helps!

Thanks,
Rim.

View solution in original post

4 REPLIES 4
Rim LANDOLSI
ST Employee

Hello @Riya  and welcome to the community,

 

The problem of the NonSecure_Init() function hitting the secure region instead of jumping to the non-secure region is due to improper memory allocation of secure and non-secure.
According to your configuration, it looks like both your banks are configured as secure. Try to change this:


SECWM2_START value = 0x01

SECWM2_END value = 0x00

apply and save and try to debug.


Check your jump address in the secure firmware, it should be the start of your bank 2 address 0x08100000UL, which is not the case as your CubeProgrammer configuration is for bank 2.

Hope this helps!

Thanks,
Rim.

Hi @Rim LANDOLSI ,

Thank you for replying to my post !

The above solution resolved my Hardfault in NonSecure_Init issue ,but in Non secure region I have configured for FreeRtos.

It's going to the infinite loop in function prvInitialiseNewTask().

Can you please help me resolve this issue.

 

Riya_0-1712143424772.png

I have attached my linker file for secure and non secure in .c format.

Thank You.

 

 

 

 

Hi @Riya ,

Glad to hear this has solved the problem.

Could you provide the FreeRTOS task configuration you have created?

Thank you.

 

Hi @Rim LANDOLSI 

Thank you for replying to my post !

I am attaching my FreeRtosConfig.h file of Non-secure region.